Glossary

A B C D E F G H I J K L M N O P Q R S T U V W X Y Z #

TCU

Telecommunications Connection Unit

TE

Transmission Equipment

Temporary overvoltage (TOV)

Temporary overvoltage may be present at the surge protective device for a short period of time due to a fault in the high-voltage system. This must be clearly distinguished from a transient caused by a lightning strike or a switching operation, which last no longer than about 1 ms. The amplitude UT and the  duration  of  this  temporary  overvoltage  are  specified  in EN 61643-11 (200 ms, 5 s or 120 min.) and are individually tested for the relevant SPDs according to the system configuration (TN, TT, etc.). The SPD can either a) reliably fail (TOV safety) or b) be TOV-resistant (TOV withstand), meaning that it is completely operational during and following temporary overvoltages.

Thermal disconnector

Surge protective devices for use in power supply systems equipped with voltage-controlled resistors (varistors) mostly feature an integrated thermal disconnector that disconnects the surge protective device from the mains in case of overload and indicates this operating state. The disconnector responds to the “current heat“ generated by an overloaded varistor and disconnects the surge protective device from the mains if a certain temperature is exceeded. The disconnector is designed to disconnect the overloaded surge protective device in time to prevent a fire. It is not intended to ensure protection against indirect contact. The function of these thermal disconnectors can be tested by means of a simulated overload / ageing of the arresters.

TMA

Tower-Mounted Amplifier

TO

Telecommunications Outlet

Total discharge current Itotal

Current which flows through the PE, PEN or earth connection of a multi-pole SPD during the total discharge current test. This test is used to determine the total load if current simultaneously flows through several protective paths of a multipole SPD. This parameter is decisive for the total discharge capacity which is reliably handled by the sum of the individual paths of an SPD.

TOV

Temporary Overvoltage