3.3.3.3 Lightning strikes to supply lines
For direct lightning strikes to an incoming line we have (Equation 3.3.3.3.1):
[equation](3.3.3.3.1)
Where NL is the annual number of surges on the line section with a maximum value of at least 1 kV.
CI is the installation factor of the supply line (Table 3.3.3.3.1) which takes into account whether an overhead line or a buried cable is concerned. If there is a high-voltage transmission line rather than a low-voltage transmission line within the area AL, the transformer required in this case reduces the level of overvoltage at the point of entry into the structure. In such cases, this is taken into account by the line type factor CT (Table 3.3.3.3.2). Finally, CE is the environmental factor (Table 3.3.3.3.3) which defines the building density near the supply line and thus the probability of a lightning strike.
The collection area AL for direct lightning strikes to the supply line (Figure 3) is calculated as per equation 3.3.3.3.2: