Skip to main content

5.2.6 Calculating the protected volume

The determination of protected volumes is a central component of the planning and validation of lightning protection systems. It is used to assess whether all relevant parts of the building and technical installations are within an effective protected volume, which is defined in accordance with the selected lightning protection class. The calculation is performed using normative methods, in particular the rolling sphere method and the mesh method, as described in IEC 62305-3.

Method for calculating protected volumes

Want to read more?

Please log in or register for free.