3.3.4.3 Probabilities of damage in case of direct lightning strikes into supply lines
The probability values PU for injuries to living beings within the structure due to touch voltages caused by a direct lightning flash to a line that enters the structure depend on the shielding properties of the supply line, the impulse withstand voltage of the internal systems connected to the supply line, the protective measures (physical restrictions or warning notices) and any isolating interfaces or SPDs provided at the point of entry into the structure in accordance with IEC 62305-3 (Equation 3.3.4.3.1):
[equation](3.3.4.3.1)
Pam describes protective measures against touch voltages, such as physical restrictions and warning notices; the values in Table 3.3.4.1.1 apply again. If more than one protection measure is taken, the value of PU is the product of the relevant values.