3.3.4.2 Probabilities of damage in case of nearby lightning strikes
The probability PM that a lightning flash near a structure will cause failure of internal systems in the structure depends on the measures taken for the protection of electrical and electronic installations (SPM). A grid-like lightning protection system, shielding measures, installation principles for the cables, an increased rated impulse withstand voltage, isolating interfaces and coordinated SPD systems are suitable protection measures to reduce PM.
The probability PM is calculated as follows (Equation 3.3.4.2.1):